| ADSL - Asymmetric Digital
Subscriber Line | Communication technology which allows high speed data
transmission (up to 8 Mbit/s) through the network’s copper
cables. |
| Extra-high Voltage | Electric voltage exceeding 150 kV employed in electricity
transmission. |
| Extruded Polymeric Insulation | Insulating material obtained by the extrusion of insulating
plastic material. |
| FTTH - Fiber To The Home | Last mile of connection to homes through fiber optic cables. |
| FTTP - Fiber To The Premises | Last mile of connection to buildings through fiber optic cables. |
| FTTX - Fiber To The ‘‘X’’ | Last mile of connection to specific locations through fiber optic
cables. |
| High Voltage | Electric voltage ranging between 60 kV and 150 kV employed
in electricity transmission from the transmission network to
primary distribution. |
| KV —Kilovolt | Electric Voltage measure unit equal to 1.000 Volt. |
| Low Voltage | Electric Voltage under (below or equal to) 1 kV employed in
electric energy distribution to residential and commercial
customers. |
| LS0H - Low Smoke Zero Halogen | Insulating and/or coating material for medium and low voltage
cables. |
| MCVD - Modified Chemical Vapor
Depositation | Technology for the manufacture of fiber optics consisting of a
rotating silica glass tube (preform) from which fiber optics are
obtained through a spinning procedure. Such technology
avoids direct contact between the traversing flame and the
silica glass tube. The main advantage of the MCVD technology
is that the depositing of the silica soot takes place in clean and
uncontaminated grounds. |
| Medium Voltage | Electric voltage ranging between 1 kV and 60 kV mainly
employed in energy distribution through primary and secondary
grids. |
| OEM - Original Equipment
Manufacturer | Company which manufactures and markets its own trademark
products obtained by purchasing components or finished
products from other companies. |
| OPGW - Optical Ground Wire | Overhead fiber optic cable for high voltage (telecom)
transmissions. |
| OVD - Outside Vapor Deposition | Technology for the manufacture of fiber optics consisting in a
rotating silica glass tube (preform) in which, through a flame
hydrolytic procedure, the silica soot is deposited on the outside
surface of the glass mandrel. |
| Passive Systems | Telecom transmission systems made of fiber-optic cables or
copper cables, electrical junction boxes in which either the
optic or electric impulse is passive and not elaborated. |
| P-Laser | Single step production procedure consisting in the combination
of different innovative modules. One of the most important
modules consists of isolation, based on extruded thermoplastic
materials, which allows employment of more competitive
production procedures, for example the insulating procedure in
XLPE. |
| PMD - Polarized Mode Dispersion | Parameter measuring signal dispersion related to the
polarization in a fiber optic. |
| Power Transmission System | Transmission energy system consisting of cables, connections,
terminations, installation and protection of urban projects and
related testing procedures. |
| PVC - Polyvinyl Chloride | Thermoplastic material for insulation/external coating of
medium and low voltage cables. |
| Umbilicals | Cables made of electric conductors and flexible tubes (plastic
or metallic) used to link offshore oil platforms to submarine oil
extraction systems. |
| VAD - Vapor Axial Deposition | Technology for the production of fiber optics consisting of the
manufacture of a rotating silica glass tube (preform) by
depositing the glass soot on the bottom end of the rotating
silica rod. The preform is continuously pulled upwards during
the process due to the growth at the bottom end. |
| Wire rod | Cylindrical metallic rolled section (copper or aluminum) from
the drawing of which basic wires are obtained. These basic
wires are used for the manufacture of conductors, by a ropelaying
procedure. |
| XLPE - Cross Linked Polietilene | Electric insulating material made of polymeric chains tied up by
chemical bonds (cross-linkage). |